Hi
We are using ISO7340-Q1 in our design. We would like to know the maximum current consumed from the side 2 (output) of the device when powered with 3.3V. The maximum signal frequency for the application is 20kHz.
As per the datasheet (Sec 7.12) the maximum current consumed at the output supply (3.3V) is 3.6mA. Is this correct?
Is there any other specification that i am missing which will cause the current consumed on side2 of this device more than 3.6mA?
The current consumption is a critical for our application. Please let us know if there is any other possibility that this device will consume more than 3.6mA on side2.
Thanks
Sudheer