Other Parts Discussed in Thread: ISO7741EVM
Hello. I am a first time user using the ISO7721FQDRQ1 part. This is the 8 pin part. I am getting no output. I have a 20KHz, 3.3V square wave going into pin 3. Pin 1 is connected to the 3.3V supply. Pin 4 is connected is connected to the 3.3V ground. Pin 8 is connected to the 2.5V supply and pin 5 is connected to the 2.5V ground. I have tried pulling the output up (10K) and also pulling it down to 2.5V ground and still nothing on the output. Any help would be greatly appreciated!
Mark