This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1212: DO-160 related question for 600V transient withstand capability

Part Number: ISO1212


A question from my customer:

Looking at the ISO1212  as a potential solution.  Any idea how this would hold up against lightning pin pulses from DO-160?

Details in the attached PPTX file.

ISO1212 600V pulse DO-160.pptx

Thanks!