This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7760-Q1: ISO7760-Q1 Viowm difference vs. ISO7710-Q1 on datasheet?

Part Number: ISO7760-Q1
Other Parts Discussed in Thread: ISO7710-Q1

Dear team,

I know ISO7710-Q1 is 1-channel version of ISO7760-Q1.

But ISO7710-Q1 Viowm(Maximum working isolation voltage) DC is 1414V. On the other hand, ISO7760-Q1 has Viowm DC is 2121V.

I am looking for 1 or 2 channel digital isolator which has over 2kV DC Viowm.

Does your team have any plan to develop this kind of device in the future?

Thank you.

Regards,

Oliver Kim