This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7761: Absolute voltage rating of signal input pin

Part Number: ISO7761

Hello team,

My customer have a question that does it violate the absolute rating of the VCC supply voltage is 3.3V and the signal input voltage level is 5V?

I think it is not allowed since the absolute input rating in this case will be 3.3V+0.5V, is my understanding correct?

Thanks very much.

Vincent Chen