Other Parts Discussed in Thread: ISO7041, ISO7763
Dear TI product management,
we would be very interested in an ultra low power digital isolator like the new ISO7041, but with the following specifications:
- Providing a continuous working voltage DC isolation of at least 1500Vdc over 20 years
- Supporting 5.0V supplied components (not only 3.3V)
- 6 channels instead of only 4 (directions: 6/3)
- Automotive AEC-Q100 qualified and temperature range of -40 to +125°C at least
Is there any plan to provide such a device, at least fulfilling the wishes in position 1 and 2? Any information would greatly help our design considerations and decisions.
Best regards
Vincent