Part Number: ISO3086
Other Parts Discussed in Thread: ISO1452, ISO1412, ISO1432
Hello everyone!
I designed a board that uses RS485 communication protocol and I have an issue when trying to make it work as full-duplex.
Every time I try to send data without disabling receiver, I receive a start bit and nothing else. Then, my uC understand that a new byte has arrived so it tries to process it.
The workaround I implemented is to turn receiver off when transmitting (it's like a "manual" half-duplex), but that's not what I am aiming to since I chose this IC because of its full-duplex feature. I measured the signals with an oscilloscope and I realized that everytime I sent a message, there's a small signal on the receiver side of the IC (RX and RX' are not connected to anything).
My question is: is it the way it works? Should I turn the receiver off everytime I send a message?
Thanks!