As the title requests, what is the maximum input rise/fall time for the inputs on the ISOW784* series of parts? I see the typical/maximum output rise time in the datasheet, but cannot seem to find the input rise/fall time limitations.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As the title requests, what is the maximum input rise/fall time for the inputs on the ISOW784* series of parts? I see the typical/maximum output rise time in the datasheet, but cannot seem to find the input rise/fall time limitations.
Hi Dan,
Essentially, what I'm asking is how long an input signal can take to cross the metastable region, in-between "Input Pin Rising Threshold", Vith, and the "Input Pin Falling Threshold", Vitl. Per TI Application Report SCBA004D, a too-slow rise time can result in excessive current being drawn, and is generally undesirable. However, I would like to slow the rise time of my signal as much as practical to reduce radiated EMI.
It looks like the ISOW784x series may have Schmitt-trigger inputs, eliminating the metastable region, but that feature is not mentioned in the datasheet; it is only implied in the "Pin Configurations and Functions" drawings.
Hi Donald,
Sorry for the delay. Yes I can confirm that the inputs have hysteresis and that this should not be an issue with the ISOW784x devices.
Best regards,
Dan