This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW7821: How to use the ISOW7821 to be a 1T1R isolation RS232

Part Number: ISOW7821
Other Parts Discussed in Thread: ISOW7842

hi sir

How to use the ISOW7821 to be a 1T1R isolation RS232

thanks

  • Hi Alex,

    ISOW7821 is a digital isolator (with integrated DC/DC converter) whose input / output voltage levels are as per digital CMOS logic. An RS-232 transceiver can be used along with ISOW7821 to achieve isolated RS-232 solution. Please refer to the below reference design that implements RS-232 using ISOW7842. The design uses ISOW7842 to implement 2T2R while for 1T1R, ISOW7821 would be sufficient. Let us know if you have any questions, thanks.

    Regards,
    Koteshwar Rao