Other Parts Discussed in Thread: SN6501, SN6505D-Q1, SN6505B-Q1, SN6505A-Q1
Hi
What is the difference between SN6501-Q1 and SN6505-Q1?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
What is the difference between SN6501-Q1 and SN6505-Q1?
Thanks!
Hi Neal,
Thank you for posting to E2E! There are quite a few differences between these two devices, so I will summarize the main points. If there is a specific parameter you are interested in, please let me know to elaborate.
SN6505 is an improvement of the SN6501 in terms of current-sinking capability: SN6505 can sink 1A of current, allowing for up to 5W of isolated power transfer while SN6501 can sink a max 350mA, allowing for 1.75W of isolated power transfer.
SN6505 also has features built in that SN6501 does not, including:
Are you currently using an SN6501 or SN6505?
Thank you,
Manuel Chavez