Hi
Need your help to recommend, two-way transmission, with isolation, without EN PIN, can replace the ADN4650 LVDS;
The search found that ISO7820LL seems to be more suitable, but our CPU does not enable the trigger signal, and the program does not define the enable port. The original design is an isolation transformer, so the trigger signal is not enabled. The EN PIN of the ISO7820LL requires a high and low power Level control;
Thanks
Elsa Duan