This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7763-Q1: Can ISO7763-Q1 connects 2 different level of voltages?

Part Number: ISO7763-Q1

Hi Team,

As title, can  ISO7763-Q1 connects different level of voltages?

ex: VCC1=5V ; VCC2=3.3V .

BR
Kane