Hi,
I see that EN pin floating can enable the output, so there should be internal pull up resistor connecting EN pin to VCC. What's the value?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I see that EN pin floating can enable the output, so there should be internal pull up resistor connecting EN pin to VCC. What's the value?
Hi Howard,
The pull-up resistor value is 2MΩ as given in the datasheet I/O schematic diagram (also copied below). If you are using the device in a noisy environment, then we recommend you to use an external strong pull-up resistor (4.7kΩ) connected to EN pin as against the weak internal pull-up resistor. Thanks.
Regards,
Koteshwar Rao