Other Parts Discussed in Thread: ISO7741, ISO7740
hi sir
I Like the ISO7041 Low power consumtion
but, do you have 5kv ver?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Chen,
The equivalent part for ADuM2400 will be ISO7740 which offers 5kVrms of isolation withstand voltage and has similar power consumption. Please do note that ADuM2400 is not an ultra-low power device and so is the ISO7740. We do not have ultra-low power device available in 5kVrsm isolation voltage. Thanks.
Regards,
Koteshwar Rao
hi sir
but the power consumption, ADI better than TI
ADUM2400 in 3 V operation
0.7 mA per channel maximum @ 0 Mbps to 2 Mbps
ISO7740 in 3v operation Low power consumption, typical 1.5 mA per
channel at 1 Mbps
Hi Chen,
I agree there are differences in current consumption between ADuM2400 and ISO7740, this is primarily due to the architectural differences between the two devices. ADuM2400 is an older family device and uses an older architecture that consumes lower current whereas ISO7740 uses the newer and more robust on-off keying (OOK) architecture and hence consumes relatively higher currents. Hence, I recommend to consider the latest and more robust architecture device and not the older generation ones. Thanks.
Regards,
Koteshwar Rao