Dear Sir/Madam,
I would like to implement level translation with a digital isolator, ISO7761. As the connection is to FPGA which the data rate could reach 400MHz, below are the scratch of the connection: VCCI = 3.3V ,GNDI =0V and VCCO = 2.5V , GNDO= -2.5V. Will this work?
Best regards,
kpk