This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1042-Q1: More documentation on the "Meets the ISO 11898-2:2016" feature.

Part Number: ISO1042-Q1

In the related thread Lucas_Schulte9 posted, that he has some additional informations on the ISO 11898-2:2016 test standard for the ISO1042-Q1 which cannot be shared on the forum.

I would also be interested in this information

I should state a compliance to the ISO 11898-2 standard of my design, but i want to avoid too much measurements due to effort.

So any more information on the feature in the Datasheet "Meets the ISO 11898-2:2016 physical layer standard" would help me in the justification for that.

Thank you,

Sebastian