Part Number: ISO7221B
Other Parts Discussed in Thread: ISO6721, ISO7721
What is the frequency of the ISO7221B Internal oscillator?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yuta,
I am assuming you are referring to the oscillator block shown in the block diagram under section 8.2 of ISO7221B datasheet. The frequency of this oscillator is ~100kHz. Let me know if there is any concern that customer has on this internal clock.
ISO7221B is one of our older family of digital isolators. I would recommend customer to use the latest generation of digital isolators to offer much better overall performance. ISO7721 and ISO6721 are our equivalent latest digital isolator devices that are pin-compatible to ISO7221B. Thanks.
Regards,
Koteshwar Rao
Hi koteshwar,
Thank you for your reply.
I am referring to the block diagram under section 9.2 of ISO7221B datasheet.
I understand that the frequency is 100kHz.
I will consider ISO 7721 or ISO6721, too.
Best Regards,
Nishie