Hi team,
My customer is using SN6501 to do 5V-5V isolated power as below topology. But when they do short-circuit test(short Vout to GND2), they found VCC input current increase rapidly and the SN6501device burns out. So I want to check if SN6501 has any internal over-current protection function? If it doesn't have, how should we deal with the short-circuit test? Please note customer doesn't want to add a LDO after T2 so we cannot reply on the LDO to do over-current protection. Thanks.
Best regards,
Wayne