Dears
First, the output is disabled, the input is low, and then the output is enabled, but the pulse waveform shown in the figure above will appear.
The main reason is that it is not clear why the low level is input, and there is a high level pulse when the output is enabled?
Do you need to use the default low level, ISO7740F?
Thanks
Elsa Duan