Other Parts Discussed in Thread: ISO7762,
Hi,
We are currently working on a design that is using ISO7740 and ISO7762 to create a 3kV isolation barrier. The requirement spec we must meet references IEC/EN61000-4-5 (surge) and IEC/EN61000-4-4 (fast Transient) test methods. There is no specific mention in the datasheet about these standards, only a mention about the EMC robustness. "the ISO776x family of devices has been significantly enhanced to ease system-level ESD, EFT, surge, and emissions compliance."
Can you advise if these devices are suitable for the standards mentioned? Is there some test data you can share to back up the statement?