Other Parts Discussed in Thread: ISO1042-Q1, SN6501
Hello,
I need to have a 5v to isolated 5V supply in my application, the datasheet recommends transformer both with and without LDO requirement based on the turns ratio.
I would like to know if there are any disadvantage of having without LDO on the sec of the transformer to achieve 5V- 5Viso requirement (by using 1:1.1 transformer) as this is an unregulated output.
The load operating current will be 5mA to 75mA.
Looking forward to hear from you soon. Thanks in advance.
Regards,
Anand M