Part Number: ISO7742-Q1
Other Parts Discussed in Thread: ISO7742
Hi Team,
My customer is using ISO7742F-Q1. For ISO7742F-Q1, Do you have more detailed information of IIH, IIL.
What is the min, typ value of IIH.
What is the max, typ value of IIL.
What is the max, typ value of IIL., IIH. at other input voltage?

Another question, if input pin is open. Then how can the output to keep low? Because the leakage current maybe -10uA from the above table. For example, if assume the input resistance 250kohm. Then 10uA*250kohm=2.5V. This is not a certain input. So the output will be undetermined?


Thanks.