My customer has a question regarding the input voltage and isolated output voltage of ISOW7741. That is whether the integrated isolated dc/dc converter can boost the voltage (It is shown in the datasheet that the input voltage range is 3V to 5V).
For example, when the input voltage is 4.5V, the isolated voltage can also be 5V, is that correct?
Regards,
Xiaoying