Hi ,
need to understand device behavior when ISO get a very low frequency signal on the input that need to be acquired promptly. If the input is stable for more than 100ms and an impulsion is applied on the input does this information is instantly provided to the output or the output is delayed due to refresh rate because of the BF mode is activated?
DR max being 4Mbps while FR max being 10Kps according to the DS.
Thanks