Dear TI..
I'm using ISO1042-Q1.
By the way, the following waveform(Fig.#1) is checked.
Why did the last waveform level come out high?
(The micro-controller is using STM8AF5286.)
Still, I would like to know the detailed reason.
Please give me a clear answer.
The results I looked for.....
(1) In my opinion, because of the CAN-FD difference....
(2) No problem in operation even when used as it is.
[Fig.#1]