This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1042-Q1: ISO1042-Q1 CAN communication waveform issue???

Part Number: ISO1042-Q1

Dear TI..

I'm using ISO1042-Q1.

By the way, the following waveform(Fig.#1) is checked.

Why did the last waveform level come out high?

(The micro-controller is using STM8AF5286.)

Still, I would like to know the detailed reason.
Please give me a clear answer.

The results I looked for.....

(1) In my opinion, because of the CAN-FD difference....

(2) No problem in operation even when used as it is.

[Fig.#1]