I have a design using a ISO1430BDWR 485 Isolator.
I'm already testing the chip using boundary scan to exercise the R, /RE, DE, and D lines.
I'd like to test the A and B lines at the connector on my board. Due to the complexity of the controlling firmware, I'm unable to just send or receive an RS-485 message.
Testing the chip itself is completed, but now I want to test the connector where my A and B lines leave the board.
I have the ability (through boundary scan) to set the A and B lines (by setting the TXD line). I was thinking about setting TXD High, reading the voltage between A and B, and then setting TXD Low, and measuring the voltage again. I would expect the voltage to be positive for one reading, and negative for another. I'm having trouble finding what that voltage should be.
I have 3.3V going to VCC1 on the chip, and 3.3V (Isolated) going to VCC2. I need to document why the level is what should be expected either by having a reference document or an equation.
Thank you.