This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7341C: VCC2=310V GND2=305V. Can it work

Part Number: ISO7341C

Dears,

Our customer are using ISO7341C, he want to use following schematic, the voltage of VCC1=3.3V, GND1=0V, VCC2=310, GND2=305V, the reference voltage of OUTA, OUTB, OUTC and IND are GND2=305V. The chip could work or not? 

Regards,

Ricardo