This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO150 alternate device

Guru 11165 points

Replies: 9

Views: 2763

Hello,

Our customer used the ISO150.

The customer start to new design, but the ISO150 is NRND.

Could you tell me the recommend device instead of the ISO150?

Best Regards,

Naoki Aoyama

  • Hello Naoki,

    If you are looking for basic isolation please use ISO7321C and if you need reinforced isolation please have a look at ISO7821. Both of these families have devices with single channel up to quad channels, you can find more details at the below link.

    www.ti.com/.../overview.page

    Regards,
    Koteshwar Rao
  • In reply to Koteshwar Rao:

    Hello Koteshwar,

    Thank you for your reply.
    I will offer the customer both devices.

    Thanks,
    Naoki Aoyama
  • In reply to Koteshwar Rao:

    Hello Koteshwar,

    Please recommend it, There are similar IOS150?

    If I need bidirection and isolation function, in GPIO.

    Thanks.

  • In reply to Lin Tim:

    Hello Lin,

    If you are looking for a bidirectional device, please have a look at ISO1540 / ISO1541. Both of these isolators offer bidirectional functionality. Let me know if you have any other requirements. Thank you.

    Regards,
    Koteshwar Rao

  • In reply to Koteshwar Rao:

    Hello Koteshwar,

    can I use the GPIO signal in the ISO1540/ISO1541 ?
    Di ISO1540/ISO1541 not only be used I2C ?
    thanks.
  • In reply to Lin Tim:

    Hello Lin,

    The device is designed to support any bidirectional communication requirement including I2C provided datarate is less than 1Mbps and I/O thresholds of ISO154x meet the device it is interfaced to. Let me know more details about your application and if there are any specific requirements so that I can comment if there is any concern. Thanks.

    Regards,
    Koteshwar Rao

  • In reply to Koteshwar Rao:

    Hello Koteshwwar,

    Thank you for your reply.
    I just want to detect or control the external signal from the CPU's IO PIN(1.8V),
    So I need to isolate Bidirectional interface.
    If it can provide higher voltage(12V) better. Thanks.

    Regards,
    Tim Lin
  • In reply to Lin Tim:

    Hello Lin,

    For your bidirectional requirement ISO1540 / ISO1541 would be the best device. ISO154x operates from 3V to 5.5V, if you requirement is to support higher or lower voltages than what ISO154x supports you will have to use a level translator to be able to support voltage levels. Thanks.

    Regards,
    Koteshwar Rao
  • In reply to Koteshwar Rao:

    Hello Koteshwar,

    Thank you for your reply.

    Regards,
    Tim Lin

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.