Hello Team,
I have 2 questions.
(1)Which of the following is the type of insulation of ISO7221C?
a) basic insulation
b) double insulation
c) reinforced insulation
(2)What is the insulation distance of "ISOLATION CAPACITOR"?
Is it spec below?
- DTI(Distance through the insulation) : 0.008mm(min)
Best regards,
Kato