This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7321C: ON-OFF keying or Edge detection

Guru 25540 points

Replies: 1

Views: 718

Part Number: ISO7321C

Hi all

Would you mind if we ask ISO7321C?

Is this device ON-OFF keying or Edge detection?
It seems that this device type is Edge detection.

Kind regards,

Hirotaka Matsumoto

  • Hi Hirotaka,

    Yes, ISO7321C works using the Edge based architecture.
    ISO7721 is our latest digital isolators based on the ON-OFF keying architecture.

    Regards,
    Anand Reghunathan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.