This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7321C: Different voltage supply on ISO7321

Intellectual 1590 points

Replies: 1

Views: 359

Part Number: ISO7321C

Hi Expert,

Can ISO7321/ISO7841 work under we provide 5V supply to VCC1 and 3.3V to VCCO?

Best regards,

Eric Lai

 

Field Application Engineer

Texas Instruments Taiwan Limited

O: +886-2-2175-2582

M: +886-909-262-582

E-Mail:Eric.Lai @ti.com

  • Hi Eric,

    Yes, ISO7321, ISO7841 & most other digital isolators at TI can operate at 5V VCC1 & 3.3V VCC2. Please note that VCC1 and VCC2 supply voltages can independently be supplied with any voltage in their operating voltage. For ISO78xx & ISO77xx, VCC1 & VCC2 can be anywhere between 2.25V & 5.5V independently. Thanks.


    Regards,
    Koteshwar Rao

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.