Hello support team,
I have some questions about ISO724x series.
I think that the EN pin of them should be fixed at 'H' level when using them in the always enabled state.
In Figure 19 on page 27 of the data sheet, Figure 20 on page 28 and , Figure 22 and 23 on page 28, the ENx pins are pulled up directly to Vccx.
On the other hand, in Figure 26 on page 30, the ENx pins are pulled up to Vccx via 4.7 kΩ of series resistors.
In the former datasheet (eg. Rev. M), the pull-up circuit via 4.7 kΩ was not described.
[Question]
1. Which is recommended, whether to be pulled up directly or via 4.7 kΩ of series resistor?
2. Why 4.7 kΩ of series resistor is needed?
What kind of case requires a 4.7 kΩ pull-up resistor?
Sincerely,
M. Tachibana