I have 7 ISO35T's on one board. My design is very very close to the reference design. The differences in my design are:
- I have DE tied high, and /RE tied to ground
- I have all of the isolated grounds tied to each other (these will be tied to an earth ground) The isolated grounds are not connected to the A side ground (or anything else).
I just recieved my prototype boards back, and when I try to power it up, the on-board regulator goes into current limit. Thinking there may be an issue with the regulator, I bypassed it with a bench supply, and it also goes into current limit, and the voltage drops to around a volt. The ISO35T's are all getting warm to very warm (depending on the current that I allow them to draw). I have not allowed them to get hot. Nothing else on the board is warming up except for the ISO32T chips.
I lifted pins 1 & 2 that drive the transformer on each of the devices, with no difference. I lifted the +3V3 pin on the center of the transformer on the non-isolated side, with no difference. Evidently the chip itself is drawing the current since the driver for the transformer is disconnected.
Does anyone have any idea what is going on? Is it OK to tie all of the isolated grounds together?