Hi,
I am evaluating TI ISOW7840 for my application .
The Query is Input side is 5V and 3V which are currently Isolated. If I short the grounds then I can give 5V or 3V as input and output is always 3.3V DC in ISO7840 IC. The efficiency is around 43% . If I use 5V input the input current will be less for same output power.
But I want to connect pin 4 and 5 which are digital input to a Microcontroller which as Vcc of 3.0 V DC. Can i use 5V DC input to ISOW7840 IC and pin 4 and pin 5 of this IC connected as input to a Microcontroller pin which is operating at 3.0 VDC . The output of this IC is be 3.3V DC only for both 5V or 3V DC inputs.
Regards
Harish