Other Parts Discussed in Thread: ISO1541, ISO1540
What are the recommended logic HIGH and LOW input voltage levels that can be applied to the isolated I2C devices, ISO1540 and ISO1541?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The recommended logic input voltage levels for ISO1540 and ISO1541 devices for Side1 & Side2 inputs are as shown below.
| VIL1 < 0.5V | VIH1 > 0.7*VCC1 |
| VIL2 < 0.3*VCC2 | VIH2 > 0.7*VCC2 |
These input voltage levels apply to both the I2C data and clock signals. For more information please refer to the Recommended Operating Section of the ISO154x datasheet.