Hi Support team,
how SN6505 IC could prevent V-S unbalance?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Red,
Thank you for using the SN6505 and creating this post on E2E. An SN6505 + transformer system has a margin for normal operation where the transformer is not magnetically saturated (within dotted line in Figure 39) and every time D1 and D2 switch, the operating point moves between A and A' as shown in the illustration.
The SN650x family of devices feature a self-correcting factor where the resistance of output FETs increases yielding a lower voltage seen on the primary side of the transformer, Vp, but v-t imbalances can be prevented in the best way by designing systems so the SN6505 sees balanced loads. This is implemented by using transformers with equal turns above and below the center taps with the appropriate V-t products. For instructions on how to calculate this, please refer to section 9.2.2.5.1 of the device datasheets.
If you have additional questions or would like for me to check a system you are working with, please click reply and let me know! We can also continue this conversation via PM.
Cheers to the New Year,
Manuel Chavez