Part Number: ISO7220A-Q1
Other Parts Discussed in Thread: ISO7720
Hi
In my design , I would like to use ISO7220 to isolate the negetive and positive signal, the signal is send to MCU which is in the positive voltage domain. Is the function right ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO7220A-Q1
Other Parts Discussed in Thread: ISO7720
Hi
In my design , I would like to use ISO7220 to isolate the negetive and positive signal, the signal is send to MCU which is in the positive voltage domain. Is the function right ?
Hi Liang,
This application is correct as long as the signal and GND pairs are preserved on each side of the ISO7220A-Q1 as shown in the image below.
The microcontroller's 3.3V supply can also be used to power the output side of the isolator. The input side must be powered by a 3V - 5.5V supply referenced to the input side ground, gnd2. Is a supply for this pin available?
Thank you for posting to E2E!
Manuel Chavez
Hi Liang,
This thread has been idle for the past couple weeks and it will be closed. Please feel free to post a new or follow up question using the red and yellow buttons on the top right corner of this window.
Thank you for posting to E2E!
Best,
Manuel Chavez