This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7220A-Q1: How to Isolate the positive and negetive voltage ?

Intellectual 420 points

Replies: 7

Views: 520

Part Number: ISO7220A-Q1

Hi

   In my design , I would like to use ISO7220 to isolate the negetive and positive signal,  the signal is send to MCU which is in the positive voltage domain.  Is the function right ?

  • Hi Liang,

    This application is correct as long as the signal and GND pairs are preserved on each side of the ISO7220A-Q1 as shown in the image below.



    The microcontroller's 3.3V supply can also be used to power the output side of the isolator. The input side must be powered by a 3V - 5.5V supply referenced to the input side ground, gnd2. Is a supply for this pin available?


    Thank you for posting to E2E!
    Manuel Chavez

  • In reply to Manuel Chavez:

    Hi Manuel,
    Thanks alot !
    Yes, gnd2 is avilable in the input side . I am clear about it , but I found there is another problem: the battary charge block in negetive voltage domain can not work , I need to solve it
  • In reply to liang ren:

    Hi Liang,

    What kind of problem is the battery charge block having? Is it powering on? A part number will be helpful in case there is a dedicated team to help us with that specific device.

    Regarding the previous conversation, I should have mentioned that the ISO7220A-Q1 is a very old part. Please consider designing with the newer, more capable ISO7720. The two devices are pin-to-pin compatible and the ISO7720 has higher isolation ratings.


    Thank you for your time,
    Manuel Chavez
  • In reply to Manuel Chavez:

    Thanks ,I will use ISO7720 in normal digital isolation. At the beigning , I would like to design two battary charger board , and the two board is conected in series inorder to generate negetive voltage, I can not use the input negetive power to charge the second board , otherswise using a switch to split the two board when charging , and connect when working . But this method will be difficult for battary voltage detect circut , because when charging I can use the passive balance IC to detect the battary voltage , but when discharge the balance IC has some negetive common voltage input , I think it will not work.
  • In reply to liang ren:

    Hi Liang,

    I understand that you would like to design with two battery charger boards connected at different operating times/modes. Can you please show this in a block diagram? It may be necessary for me to contact engineers in a power management team to help.


    Thank you,
    Manuel Chavez
  • In reply to Manuel Chavez:

    Hi Liang,

    Are the battery charger boards working now? Which devices are being used? I will await your response.


    Thank you,
    Manuel Chavez
  • In reply to Manuel Chavez:

    Hi Liang,

    This thread has been idle for the past couple weeks and it will be closed. Please feel free to post a new or follow up question using the red and yellow buttons on the top right corner of this window.


    Thank you for posting to E2E!

    Best,
    Manuel Chavez

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.