Other Parts Discussed in Thread: MAX3221, ISO1410, THVD1450, ISO7741, ISOW7841, SN6501, THVD1451
Hi there:
Our customer would like to use line driver / receiver and isolator combination to full-fill the RS232 & RS485.
Dose those following combination could achieve that?
RS-232: MAX3221 & ISO7721
RS-485: THVD1450 & ISO7721 or ISO1410
If it's not suitable, do we have other suggestion could provide?