This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7762: ISO7726 RoHs compliant

Intellectual 2680 points

Replies: 2

Views: 493

Part Number: ISO7762

Customer Question.

Is the ISO7762DWR  compliant to the new RoHS 2015/863/EU directive?

Thanks,

Regards,

Joe

 

  • Hi Joe,

    Thank you for using E2E forums!

    ISO7762DWR is 'Green' which means the content of Chlorine (Cl) and Bromine (Br) based flame retardants meet JS709B low halogen requirements of <=1000ppm threshold.

    Please let me check with the experts in my team to get back to you with exact details on RoHS 2015/863/EU compliance.

    Best regards,
    Manasa

  • In reply to Manasa Gadiyar10:

    Hi Joe,

    TI’s semiconductor products designated as “RoHS,” “RoHS Exempt” or “Green” (defined below):

    • Contain below the restricted substances maximum concentration values in Annex II the European Union’s (EU) Restriction on Use of Hazardous Substances Directive 2011/65/EU, as amended by EU 2015/863 (“RoHS”)

    So yes, ISO7762DWR is compliant to this standard.

    Best regards,

    Dan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.