Hi team,
From ISO1050 datasheet, we can see that recommended Vcc2 range is 4.75-5.25V. But according to experiment, ISO1050 can work normally when the Vcc2 drops to 4.0V. So my question is what the Vcc2 maximum and minimum are for ISO1050 working normally. How do you get the Vcc2 range(4.75-5.25V)? And what is the potential risk if ISO1050 works below 4.75V(Vcc2) continuously?
Thanks very much!
Sophia Yao