Part Number: ISO7740
Hello guys,
One of my customers is evaluating ISO7740 on their own board for their new products.
At the evaluation, they found the secondary side output of the device outputs H level shortly (1.5V hight and 3~4us width pulse) when the secondary sode power was powered up with about 200us from 0V to 3V just after the primary side VCC (VCC1) was powered up.
Then EN2=open and INx="L" level.
The customer question is the follow.
Is it normal operation that the short pulse is output at secondaly side VCC (VCC2) powered up inspite of low INx?
Your reply would be much appreciated.
Best regards,
Kazuya.