I read on the datsheet IECEx (IEC 60079-0 & IEC 60079-11) and ATEX (EN 60079-11) is planned.
When it will be available?
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Alberto Burani said:Part Number: ISO7041
I read on the datsheet IECEx (IEC 60079-0 & IEC 60079-11) and ATEX (EN 60079-11) is planned.
When it will be available?
thank you
I was meaning certifications are planned, sorry.
Alberto,
We are still in progress on acquiring these certifications. Unfortunately, I can't share detailed information on completion estimates on the public forum.
Respectfully,
Lucas
is it possible to have this info as a private message?
We are in desgn phase and I would like to understand if this certification can meet our schedule.
Thank you
Alberto,
Yes it is possible to convey the info over private message. Accept my friend request and we can continue the discussion via PM.
All,
The ISO7041 has been formally certified for both ATEX and IECEx. More information about these safety certifications can be found in the datasheet. Certification documents can be found in the ISO7041 product folder under the Technical documentation tab
Respectfully,
Lucas Schulte