Excuse me, the input power comes from IN (1-Pin) and the output power comes from OUT(3-Pin).
1. Do I have to power VCC1?
2. EN needs to be connected to VCC1?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Excuse me, the input power comes from IN (1-Pin) and the output power comes from OUT(3-Pin).
1. Do I have to power VCC1?
2. EN needs to be connected to VCC1?
Hi Jun Wei Huang,
Welcome to E2E! ISO121x input power is derived from signals input to Pins 7 - 8, so no additional supply is needed on the input side.
Regarding the output side, Pin 3 outputs HIGH and LOW signals relative to the input signal levels. This is a data pin, not a power supply pin, so yes, power must be supplied between 2.25V and 5.5V to Vcc1 (pin 1) for proper operation.
EN pin activates the device's output pin when EN = HIGH or is left floating: this may be connected to Vcc1 or left disconnected for the device to continuously operate
Please let us know if you have additional questions.
Thank you!
Manuel Chavez