• Resolved

ISOW7841: Ground shifting

Prodigy 40 points

Replies: 6

Views: 70

Part Number: ISOW7841

In our application we are going to connect 30V battery module in series configuration to get 1000V battery pack. Each battery pack has AFE(Analog front end) and microcontroller inside.So we need to establish  isolated SPI communication between the AFE and microcontroller . That means each module has AFE, Microcontroller and Isolated SPI IC. So we chosen ISOW7841.Please let's know  is this ic capable of working with the ground shift .That means when battery module are connected in series ground shift is going to happen,and AFE ic is capable of seeing that ground shift. But i don't know about ISOW7841. Please tell me this ic is capable or not.