This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7721-Q1: ISO7721-Q1 and ISO7221A-Q1 EMC

Part Number: ISO7721-Q1
Other Parts Discussed in Thread: ISO7221A-Q1,

Hi team,

Good day.

Our customer would like to switch from ISO7221A-Q1 to ISO7721-Q1 since it offers a 100Mbps data rate compared to 1Mbps of ISO7221A-Q1. Since both devices have the same pin-out, is there any impact for automotive-grade EMC STD qualification testing if the same PCB layout is used?

Regards,
Carlo