This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1042: USB to CAN

Part Number: ISO1042

I am looking for an IC or a design solution that will convert USB to CAN with 4kV insulation and 8kV creepage. ISO1042 looks OK, but it is not USB.

  • Hi Magnus,

    Thank you for posting to E2E! TI does not have an isolated CAN to USB IC or solution at this time. ISO1042 or ISO77xx devices meet the 4kV isolation voltage and 8mm creepage/clearance requirements, however a discrete solution would require both CAN and USB controllers (or an MCU integrating these features), and we do not have such a design available.

    What is the application for a solution like this?


    Respectfully,
    Manuel Chavez