Other Parts Discussed in Thread: SN6501-Q1
Hi Expert,
When customer using SN6505B-Q1 for traction inverter.But they meet a thermal issue. Here is the schematic:
At fist, customer follow the reference design of SN6501-Q1; The output current is 10 mA. Customer need this device need work well under 105C environment.
Due to the efficiency difference, we change SN6501-Q1 to SN6505B-Q1;
(Note: TPS76350-Q1 can't work well at 105C, we also change to TPS7B6950-Q1);
When we put the board in to 105C environment for 30 minutes, it can work well. But when the test time extend to 120 minutes, the diode temperature ramp up to 130C. Then SN6050B-Q1 enter to over current protection. When we change the diode to 1N4148 (MBR0402L was used in this board before). It can work well.
Could you analyze it for us? Could you recommend several diode to us?
This is a urgent case for customer. I appreciate it if you can help.
Best Regards
Songzhen Guo