Other Parts Discussed in Thread: TCA9517A, , TCA9548A
I have the following connections -> #1 ISO1540 side 2 going to the B-side of a TCA9517A (through a linking cable "A"). The A side of the TCA9517A goes trough PCB trace capacitance to a TCA9548A switch. Each of the 8 outputs of the switch go to Side 1 of another ISO1540, #2.
We think that we've violated the input capacitance (40pF max) of the #2 ISO1540 since the output capacitance of the TCA9548A is 28pF + 7.5pF = 35.5pF when the switch is closed along with the #1 TCA9517A output capacitance (~ 13pF max) + the input capacitance of the # 2 ISO1540 side 1 (7pF typ) = 55.5pF and that's without trace or cable capacitance.
Please confirm this is correct. If so, do we have an alternate solution to fan out 8 I2C isolated I2C connections?
Is it ok to interface to the TCA9548A as described?